Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

L6480 EVAL and X-NUCLEO-IHM02A1

Hello,I am planning to drive 3 Stepper motors using ST drivers. Currently, I would like to use L6470 for 2 motors and L6480 for the remaining one. I am planning to develop a test setup using following EVAL boards from ST, X-NUCLEO-IHM02A1 - Drive 2 s...

sps by Associate
  • 1193 Views
  • 0 replies
  • 0 kudos

Flash Default Firmware STA8100_D0

I am using the GNSS receiver STA8100GA and the EVAL board EVB-TAPP_E1. Yesterday I wanted to change the protocol from RTCM to NMEA. To do this I used the FW configuration window to set RTCM_OB_OFF_SWITCH = 0 & RTCM3_ON_OFF_SWITCH = 0 and NMEA_OVER_UA...

Resolved! ISO808 Ground connection

in ISO808 I have connected +5V at VDD and +28V at VCC. In my application isolation is not required so is it ok if I short GNDDD and GNDCC with filter?

sabari1_0-1688560038192.png
sabari1 by Associate III
  • 2598 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.