2023-07-05 12:14 AM
How can we differentiate between Power ON Reset vs MCU Reset initiated by an external watchdog device?
I mean is there a Memory Area in STM8AF5288 MCU that retains state after MCU Reset compared to Power ON Reset?
I cannot find the source of the MCU Reset as the External Watchdog output is connected to the MCU Reset pin.
2023-07-05 7:11 AM
You can't. Use the internal watchdog
If you want to find the source of the MCU reset, disconnect the external watchdog.
2023-07-05 11:23 AM
Could we use the noinit ram section variables to distinguish between external watchdog applied MCU Reset versus Power ON Reset? Is it possible with STM8AF5288 MCU ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.