2023-07-07 6:26 AM
I am using the GNSS receiver STA8100GA and the EVAL board EVB-TAPP_E1.
Yesterday I wanted to change the protocol from RTCM to NMEA. To do this I used the FW configuration window to set RTCM_OB_OFF_SWITCH = 0 & RTCM3_ON_OFF_SWITCH = 0 and NMEA_OVER_UART_ON_OFF to 1 and NMEA_UART_PORT_NUMBER to port0.
After applying the new configuration and reconnecting the device, Teseo Suite can't detect my receiver.
The receiver is also not detected when I add it manually with all possible configurations.
So I think I've done something wrong.
Is there a way to flash the default firmware without Teseo Suite (because I can't find the device in the FW configuration panel)?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.