Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Breakpoint on TRAP interrupt gets removed!

I'm using the ST Visual Developer V4.3.12 and trying to do what sample stm8s code suggests, namely set a breakpoint on TRAP interrupt (which I am 99% sure it tripping because of a bug in my code).  The debugger keeps "moving", i.e. removing the break...

Initialized const pointer

How do I correct this code so that the pointer is a constant and not place into RAM?```const typeOfVariable Variable = DEFINED_VARIABLE_VALUE;const typeOfVariable *pVariable = &Variable;````pVariable` keeps ending up in RAM and I've run out of ideas ...

Resolved! Create Time delay using 555 timer IC

Hi, I have create one adjustable multi vibrator circuit using 555 timer IC my aim is to achieve two things  1.Basically 555 timer IC output is Rectangular wave my aim is achieve ontime of one pulse 0-10us(Micro seconds) time delay  2.Another one is o...

Vignesh_V by Associate II
  • 2631 Views
  • 1 replies
  • 0 kudos

Resolved! DRM is missing STM for DFU

Hi, When I connect a digital radio via the USB cable, Device Manager should show under USB: STM Device in DFU mode. However, it doesn't. Instead, I have an Other Devices: Digital Radio in USB mode, with a yellow triangle with black exclamation point....

Resolved! Help to identify the part

Hi all and good time :hand_with_fingers_splayed:can U help me please?i'm confused about this part with the (UM smd code),i searched a lot on google and but i found only 2 parts with this smd code... (zener diode and tvs diode) !!:thinking_face:my fir...

UM2.jpg IMG_20240427_091348.jpg bzx84j-c5v6.png Screenshot 2024-04-27 at 11-17-48 Bourns® Chip Diodes - Bourns-SMAJ15CA-datasheet.pdf.png
mazieis by Associate II
  • 2473 Views
  • 4 replies
  • 2 kudos

How to design universal analog input circuit

Hi,I'm designing a PCB that can get 8 digital inputs and 4 analog inputs. But these inputs can be range from 3.3v to 24v. For the digital inputs I have used universal logic shifter method using comparator where I can give any voltage range of digital...

jsw2000_0-1713949440598.png
jsw2000 by Associate II
  • 4517 Views
  • 4 replies
  • 0 kudos

Resolved! M24C01-R behaviour on power-loss

I'm looking to add a serial EEPROM to a product, and have a somewhat odd situation. The device will loose power spontaneously and often (few times an hour). My question is: What happens if the M24C01-R looses power during a write operation?  I assume...

CptSlow by Associate
  • 1467 Views
  • 1 replies
  • 0 kudos

Resolved! iNEMO-M1 SW package

Hello,i have the inemo-m1 board,  bought waaay back in 2015... back then i remember i managed to work with some sample code from ST.However years have passed... and would be great to find a download location for the sample code.I have tryied searchin...

Bogdan by Senior
  • 4406 Views
  • 4 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.