Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Technical issues related to RF transistor SD2933:We want to use this transistor to drive piezoelectr

I have the following questions and need help:1. Can this transistor be used at a frequency of 900kHz? Can it only be used in frequency bands above 1MHz?2. The data sheet provides a test circuit under 30MHz conditions. We do not fully understand the f...

H_YM by Associate II
  • 16364 Views
  • 14 replies
  • 0 kudos

stwlc98 TX mode

What steps are required to set stwlc98 to TX mode?If you set 0x0020 to 01, 0x000E becomes 03.However, AC1 and AC2 do not cause burst oscillation.The Optional (TX mode only) circuit is on the board, and VOUT is connected to 5V.

Hisanori by Associate
  • 3148 Views
  • 5 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.