2019-06-22 3:04 AM
For my SensorTile, when I open the ST BLE Sensor app then create/use an app in Create Apps and tap Play, I get a "Board scanning has timed out" error message. Everything under "Connect to a device" interacts happily with the SensorTile. What's the problem?
I'm using the ST BLE Sensor app v 4.4.3 on iOS.
Thank you.
2020-04-06 12:56 AM
2020-04-13 11:13 AM
Logging does not seem to run for much longer than 1000 minutes / 2000 samples on the last test. Is there a setting for this? I see a Days/Hours/Minutes page but that is set to 0,0,1.
2020-04-14 5:43 AM
Hi @AWatt.1 , depending on the selected maximum ODR (e.g. if you selected the microphone), are you sure it's not a limitation related to the SD card capability, or to the battery -especially in case the bluetooth is connected? Is your log file sudden interrupted?
Regarding >>I see a Days/Hours/Minutes page but that is set to 0,0,1 did you selected the RTC (Date) input in you application?
Regards
2020-04-14 7:42 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.