2018-08-20 12:56 PM
2018-08-21 1:25 AM
What you mean by valid Vout? It is very difficult to define such a parameter.
The time will be dependent on the load capacity, temperature change, thermal capacity of your HW, ...
2018-08-21 5:32 PM
By valid Vout, I mean a Vout that represents current temperature reading. When supply voltage is applied, there is a steadily increasing voltage at Vout that ultimately settles at a level that represents the current temperature.
I understand the difficulty in defining the parameter. I was hoping that ST could provide some time delay based on a particular circuit scenario. Vout connected directly to some ST ADC over a trace of x width and y length. Certainly, there is some range that can be provided as a rule of thumb.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.