Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
Hi,This is my first question to the community so hello! :)I've recently started working with the LIS3DH accelerometer and I am experiencing some difficulty in interpreting the startup sequence for the device. Using the datasheet and AN3308 the startu...
When I first boot the board the accelerometer is not recognized in IIO. After a reboot it does or if I do a rmmod and then modprobe on the kernel modules.My kernel is based on the TI 4.4 kernel from the 3.02 automotive SDK. The accelerometer kernel m...
Hi! I have a custom pcb with Lsm6dsl connect to mcu (nrf52832) via i2c. I can write and read regs of Lsm6dsl well (who I am also return 0x6a). But when I try to write ODR bits in CTRL1_XL (10h) reg (for example 0x10) then I can not work,because it a...
https://www.st.com/content/ccc/resource/technical/document/application_note/group0/26/07/3f/bf/12/55/47/62/DM00402563/files/DM00402563.pdf/jcr:content/translations/en.DM00402563.pdfEquation:|Min(ST_X)| <= |OUTX_ST-OUTX_NOST| <= |Max(ST_X)|What is ST_...
Posted on February 02, 2018 at 07:06My setup is very similar to my setup in previous question: https://community.st.com/message/182613-re-motionar-initialize-function-gets-stuck?commentID=182613&et=watches.email.thread#comment-182613 SensorTile + Da...
I try to add mutex in the X-CUBE-53L1A1 SimpleRangingExamples I have defined #define VL53L1_GetI2cBus(...) CO_Mutex_get() in vl53l1_platform.c #define XNUCLEO53L1A1_GetI2cBus(...) CO_Mutex_get() inX-NUCLEO-53L1A1.cand also for PutI2cBusBut the driver...
The goal is to create the precise (and as cheap as possible) inclinometer, basing on the IMUs sensors. It should measure the angle change of the rotating wheel (speed up to 250 deg/s), with accuracy of 0.01 degree. I am not rejecting the fushion of f...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.