2019-02-26 1:30 AM
Hi,
I struggle to use the STEVAL-MKI109V3 board with Windows 10. The VCP serial port is detected, but the OS is unable to attach the right driver (a yellow exclamation mark is shown in the Device Explorer). Other STM32 boards with USB CDC do work fine.
I tried to upgrade the firmware to version 2.40.1 (included with Unico), which seemed to be succesful.
I'd be very happy for any hints on how to operate the eval kit with Win10. Thanks.
2019-02-26 5:10 AM
I have the same issue... If you advice us what we can do in order to make it works under Windows 10 it will be great. Thank you
2019-02-26 5:35 AM
You could try to play with Windows options, especially compatibility settings.
2019-03-03 10:35 PM
Hello all,
I was also facing the same issue, rather than updating the driver from device manager I resolved this issue by installing VCP_V1.5.0_Setup_W8_x64_64bits from installation folder: MEMS_Demonstration_Kit_SW_package_v8_0_WINDOWS-> Driver->STM32_vcp.
Try this let me know if it works for you.
Thank you
D.Vishnu
2019-03-04 8:24 AM
Thank you your suggestion works very good. Have a great day
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.