MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM303AGR CTRL_REG4 FS[1:0] Full Scale Selection is reversed?

Hi,Based from the LSM303AGR CTRL_REG4 FS[1:0} Full Scale Selection are (00: ±2g; 01: ±4g; 10: ±8g; 11: ±16g). I tried all settings and it is reversed. So, setting 00 is +-16g. So is this an error in the datasheet?Regards,Markel

MRobr by Associate III
  • 721 Views
  • 0 replies
  • 0 kudos

LSM6DS3, any reason not to run it on 2.5VDC supply?

We're designing the LSM6DS3 into an existing product that already uses a 2V5 supply rail. The LSM6DS3's spec sheet says that running it at 2V5 is well within spec, but all of the examples refer to a 1V8 supply. Is there any reason that a 2V5 supply i...

Using STEVAL-MKI109V3 with Windows 10

Hi,I struggle to use the STEVAL-MKI109V3 board with Windows 10. The VCP serial port is detected, but the OS is unable to attach the right driver (a yellow exclamation mark is shown in the Device Explorer). Other STM32 boards with USB CDC do work fine...

how to simulate Sent protocol ?

Hello everybody,I wanted to simulate the Sent_Protocol with a STM32 µC or simulate it as if I had a sensor. and present this with oscilloscope. Now the signal should be like a normal PWM Signal look like. I really do not know how to generate this par...

Samuel1 by Associate III
  • 2327 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.