2017-10-10 3:36 AM
Hi,
I'm using IIS2DH in my application and I am in the need of reading FIFO values registered after a threshold has been reached. For this reason using Stream-to-FIFO mode seemed perfect. But I tried it and I had some problems and doubts.
What I was trying to do was to use this configuration:
INT2_CFG = 0b00101000; //OR Event enabled, High Z, Y axes enabled
INT2_THS = 0b00011000; //24LSB = 1.488 gCTRL_REG_1 = 0b01001110, //LP 50 Hz X axis disabled
CTRL_REG_2
= 0b00001011, //Filter: normal mode HPM = 00, ft = 0.2 Hz, FDS = 1, HPIS = 1CTRL_REG_3
= 0b00000010, //OVR on INT1CTRL_REG_4
= 0b00100000, //Normal MODE, FS=+-8gCTRL_REG_5
= 0b01000010, //FIFO enabled with latch on INT2 pinCTRL_REG_6
= 0b00100000, //Int function 2 on INT2 pinFIFO_CTRL_REG
= 0b10000000,//Stream modeThe idea was to use the INT function 2 (I guess it is referret to the OR the I set in the INT2_CFG register) to toggle the INT2 pin and switch from to Stream mode to the FIFO mode, then read the FIFO overrun interrupt on the INT1 pin, read all FIFO elements through a multiple byte read command and in the end clear the INT2 pin by reading the INT2_SRC register.
In practice after reading the INT2 pin I can't see any FIFO overrun in the INT1 and I cannot know when to read the FIFO ('cause it's full-filled). I've noticed that after the initialization of accelerometer registers I get an interrupt on INT1 pin and I think it's due to the fact that FIFO overrun it's generated also in Stream mode and in FIFO mode, so when the accelerometer starts in Stream mode it will fire a overrun interrupt when FIFO is full-filled. The problem is I don't want to read any value from the accelerometer since the threshold is reached and the FIFO is filled, because this will cause my microcontroller a waste of clock operations and keeps busy the I2C bus.
I also made I try activating another threshold using:
INT1_CFG = 0b00101010; //OR Event enabled, High axes event enabled
INT1_THS = 0b00001100; //12LSB = 192 mgand enabling AOI1 on CTRL_REG_3, but I've seen that no interrupt is fired on INT1 pin after the INT2 event toggles the INT2 pin.
So my doubts are:
1) Do the latch set on INT2 function locks the entire accelerometer and not only the INT2 pin/function?
2) I also tried to unset the latch on int2 function but what I had is that the FIFO mode where never toggled. Is It because INT2 pin needs to stay at logic level 1 to make the toggle, not just a spike?
3) There is a configuration which I can set to use the accelerometer the way I need?
Thanks,
Marco
#iis2dh2017-10-23 4:02 AM
Yes, I have completely the same register settings.
It is strange it doesn't work in your case. Maybe you can try to share with me your project or the part related to the sensor, so I can have a look at it.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.