MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LIS3DH Self-test output change far from the expected

Posted on October 24, 2017 at 19:03Hello, I'm trying to perform self-test feature of the lis3dh, by following the insctruction identified in the appliacation-note  AN3308. the Self-test output change Obtained is geater than the maximum value identif...

VL53L0X seems to stuck in/after init

Posted on October 24, 2017 at 21:39Hello together,i used the stm linux driver files to create and load the driver module. This results in /dev/stmvl53l0x_ranging. I connected the vl53l0x sensor and the i2cdetect reports it under 0x29.I then wanted t...

LSM330DLC data sheet questions

Posted on November 07, 2013 at 19:32Hello, I need to configure a LSM330DLC in a way outlined in the DT0005 document.  Essentially, on data ready interrupts (INT1_A) from the accelerometer feed into the DEN_G pin, telling the gyro to push a conversio...

LIS2DH12 output x,y and z

Posted on October 20, 2017 at 10:46Hello all, my problem is the output of the x,y and z registers.The content of the registers change when moving, but only with fast movement. The values change during the acceleration. Unfortunately, after the movem...

jan n by Associate II
  • 3833 Views
  • 8 replies
  • 0 kudos

lis3dsh

Posted on October 10, 2017 at 00:07I am looking for the MTBF/FIT rate for LIS3DSHTR Accelerometer, with Confidence Level, Test Temperature and Activation Energy. Thank you.

LIS3DSH past pocessing temperature issues

Posted on October 17, 2017 at 15:56Dear all,We use LIS3DSH and we have issues after reflowing process.In fact values are not compensate correctly between -30�C to + 65�C; we have hysteresis and breaking.Measurements are out of specifications .See at...

Stream to FIFO mode and WTM interrupt generation

Posted on October 10, 2017 at 12:36Hi,I'm using IIS2DH in my application and I am in the need of reading FIFO values registered after a threshold has been reached. For this reason using Stream-to-FIFO mode seemed perfect. But I tried it and I had so...

FOR LIS2DE12, what are the HPF Settings for CTRL_REG2 (21h)

Posted on October 22, 2017 at 17:24Hi, in the datasheet for the LIS2DE12 accelerometer, page 33, the explanation of fields for CTRL_REG2 (0x21) are incomplete. There is no explanation of what the allowable values are for bits HPCF[2:1] - high pass f...

Sensortile, Firebase and a pin

Posted on October 23, 2017 at 05:47Hello, I need to upload data from Sensortile to Firebase, but firebase does not have mqtt protocol, how can I upload this data to Firebase?and another question, when I try to connect my Sensortile to an Android dev...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.