2025-03-13 3:16 PM
Hello, I have the sensortile box pro. I have used the algobuilder in the MEMS-studio to configure various data outputs (Acc, Gyr, RotationVector 6x). The sensortile isplugged in with USB. I can see those data coming into the MEMS-studio algobuilder evaluation, and I have no problem logging the data.
I want to know how can I pull the same data into a Matlab. to perform a few real-time analysis. I cannot find documentation on how the communication works. I can connect to sensortile as a serial port object. I'm assuming the baudrate is 115200. However, I don't know what commands I need to send to it for it to return those data.
Can anyone point me into the right direction?
Thanks.
2025-03-21 2:09 AM
Hi @Gawa ,
To pass the data from sensortile to the PC you have to create a flow from "expert view" with the sensors you are interested in as input, and as output you have to set “stream to USB”.
That way the sensortile will install a virtualCom on the PC, just connect matlab to that VirtualCom to pass the data.
The Data is in CSV format.
The data-log via USB will start automatically when you restart the sensortile.
2025-03-25 7:04 AM
When you say 'expert view', you are referring to the ST sensor app and not the MEMS Studio, is that correct?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.