2018-05-31 4:46 AM
Hi,
I am trying to use STM32 cube and ADXL345 ACC using SPI , this is my first time trying , and currently without luck as i am not able to read the accelerometer
This is my SPI init code :
void MX_SPI1_Init(void)
{hspi1.Instance = SPI1;
hspi1.Init.Mode = SPI_MODE_MASTER; hspi1.Init.Direction = SPI_DIRECTION_2LINES; hspi1.Init.DataSize = SPI_DATASIZE_8BIT; hspi1.Init.CLKPolarity = SPI_POLARITY_LOW; hspi1.Init.CLKPhase = SPI_PHASE_1EDGE; hspi1.Init.NSS = SPI_NSS_SOFT; hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_16; hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB; hspi1.Init.TIMode = SPI_TIMODE_DISABLE; hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE; hspi1.Init.CRCPolynomial = 10; if (HAL_SPI_Init(&hspi1) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }}
And below the code i am trying to run:
ADXL345_write(ADXL345_DATA_FORMAT_ADDRESS, &data, 1); //0x31 - resetting
ADXL345_write(ADXL345_POWER_CTL_ADDRESS, &data, 1); //0x2D - resetting ADXL345_set_bit(ADXL345_DATA_FORMAT_ADDRESS, ADXL345_DATA_FORMAT_FULL_RES_BIT); //setting 3 bit (0000 1000)? ADXL345_set_bw(ADXL345_BW_25); //0x2C BW_Rate reg: setting 0x09 - no low power, bw 1001 ADXL345_set_range_bits(1); //setting +- 4G ADXL345_set_bit(ADXL345_POWER_CTL_ADDRESS, ADXL345_POWER_CTL_MEAS_BIT); //0x2D setting 3 bit (0000 1000)- start measure?And here a sample implementation of the write and read functions:
uint8_t ADXL345_write(unsigned char address, unsigned char* adata, unsigned char n_byte)
{ uint8_t status = 1; unsigned char i;address &= ~ADXL345_RW_FLAG;
address = (n_byte > 1) ? (address | ADXL345_BM_FLAG) : (address & ~ADXL345_BM_FLAG);HAL_GPIO_WritePin (ADC_CNV_GPIO_Port, Acc_SC_Pin, GPIO_PIN_SET);
AD7689_delay();
status = HAL_SPI_Transmit(&hspi1, &address, 1, 1000);
if ( status != HAL_OK )
{ return 1; }for(i = 0; i < n_byte; i++)
{ status = HAL_SPI_Transmit(&hspi1, adata +i , 1, 1000); if ( status != HAL_OK ) { return 1; } }HAL_GPIO_WritePin (ADC_CNV_GPIO_Port, Acc_SC_Pin, GPIO_PIN_RESET);
return 0;
}uint8_t ADXL345_read(unsigned char address, unsigned char* adata, unsigned char n_byte)
{ uint8_t status = 1; unsigned char i = 0;//Wire.requestFrom((int)ADXL345_ADDRESS, (int)n_byte);
address |= ADXL345_RW_FLAG; address = (n_byte > 1) ? (address | ADXL345_BM_FLAG) : (address & ~ADXL345_BM_FLAG);HAL_GPIO_WritePin (ADC_CNV_GPIO_Port, Acc_SC_Pin, GPIO_PIN_SET);
AD7689_delay();status = HAL_SPI_Transmit(&hspi1, &address, 1, 1000);
if ( status != HAL_OK ) { return 1; }while(i < n_byte)
{ status = HAL_SPI_Receive(&hspi1, adata + i, 1, 1000 ); if ( status != HAL_OK ) { return 1; } i++; }HAL_GPIO_WritePin (ADC_CNV_GPIO_Port, Acc_SC_Pin, GPIO_PIN_RESET);
if(i == n_byte)
{ return 0; } else { return 1; }}any help will be greatly appreciated.
Thank,
Michael
#adxl345We’re moving the ST Community to a new platform to give you a better and more reliable community experience.