cancel
Showing results for 
Search instead for 
Did you mean: 

[ATT]11840

willcfj
Senior
Posted on April 06, 2018 at 01:33

SensorTile: Auto Log on power-up

All:

I have been tinkering with the SensorTile to use as-is for some data logging applications.  It wasn't my original intent, but it turned out to be so handy as-is I didn't see a need to make something ground-up for my very limited application.

For this application the double-tap to start/stop didn't make sense, I wanted the device to start logging upon turning on and then log until I switched the device off.  To make this work reliably, I made the following changes:

 - Always create a new sequence number in the log file

 - Start logging on power-up

 - Flush the file system caches on every write so at most one data sample is lost on power down.

See the post titled 'SensorTile SD Card Data Logger filename improvement' for the changes on ensuring each time a log file is created, it is a new sequence number.  The standard code always starts at 000 on every power-up, erasing anything previous.  This checks for already existing filenames and finds the first available serial number (well, up to 999 files anyway).

Attached below is the modified main.c to start logging on power-up.  To do this I created the &sharpdefine LOGALWAYS near the top.  While unrelated, I also created the ACC_RANGE &sharpdefine to increase the accellerometer range.  Too many changes, so just posting the updated main.c.  Look for wmb: for my changes to the standard 1.3.1 distribution

To minimize data loss, add the code below to the file datalog_application.c on/about line 171, in the routine DATALOG_SD_writeBuf() right after the f_write() function.  This flushes the data written to the SD card so that when power is finally removed, any data written up to that point is safely on the SD card. Bit iffy, but works quite well.

  /* wmb: do a sync to avoid any data loss due to error conditions, abort if problems */

  if(f_sync(&MyFile) != FR_OK)

  {

    return 0;

  }

Hope someone finds this helpful.

will

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Former Member
Associate II
Posted on May 30, 2018 at 14:34

Thanks for the attachment. The main.c you attached worked fine. This main.c needs to be coupled with the datalog app mod you provided or you would lose data on power down.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.