2023-03-30 10:57 PM
On the website, in the databrief it is not stated how to connect the jumpers on the steval-mki227ka, I would like to know how to enable SPI mode 1 on the evaluation kit for testing.
The problem that I'm getting is that even reading the who am I address it gives back the wrong answer.
All help will be appreciated.
Solved! Go to Solution.
2023-03-31 5:33 AM
Dear KRudo,
at the following link you can find the board schematic.
https://www.st.com/en/evaluation-tools/steval-mki227ka.html#cad-resources
In order to communicate to the device through SPI you don't need to configure jumpers in a specific mode but if you don't use Qvar feature i suggest you to close jumpers 3 with 5 and 4 with 6.
You can check the datasheet here in the section 5.1.3 to see how to issue the SPI reading.
Let me know.
2023-03-31 5:33 AM
Dear KRudo,
at the following link you can find the board schematic.
https://www.st.com/en/evaluation-tools/steval-mki227ka.html#cad-resources
In order to communicate to the device through SPI you don't need to configure jumpers in a specific mode but if you don't use Qvar feature i suggest you to close jumpers 3 with 5 and 4 with 6.
You can check the datasheet here in the section 5.1.3 to see how to issue the SPI reading.
Let me know.
2023-04-01 5:20 AM
Hey Laboz,
after some playing around I got to the result that I wanted (I was reading the register in a loop and for some reason my NRF52 DK got a little whacky and started to push all the data to high).
My follow up question is, is the device set up by default? I am trying to read the gyro, accel, and temp data without success, I am following the LSM6DSV16X datasheet with the register mapping to read the data.
I am also using the ST C source and header file from the git repository and using the functions: lsm6dsv16x_device_id_get (success),
lsm6dsv16x_flag_data_ready_get(for drdy without success),
lsm6dsv16x_temperature_raw_get(for temp data without success),
lsm6dsv16x_angular_rate_raw_get(for gyro data without success),
lsm6dsv16x_acceleration_raw_get(for accel data without success).
any help on this matter will help me a lot.
best regards,
Kirill
2023-04-04 12:44 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.