MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to change a network called in FP-AI-CTXAWARE1 package?

Hello, I recently bought the STEVAL-MKSBOX1V1 card (Sensortile.box). I would like to perform emotion recognition from speech through a convolutional network of my own creation. I downloaded the FP-AI-CTXAWARE1 package and opened the project on STM32 ...

FRana by Associate
  • 1805 Views
  • 1 replies
  • 0 kudos

LSM6DS3TR-C not generating new data

I'm using a ​LSM6DS3TR-C and polling the status register to determine when the gyro or accelerometer have produced a new value. This works fine for the most part however, if the sensor is moved quickly, it locks up and the new data sample bits in the...

ALees.2 by Associate
  • 2417 Views
  • 2 replies
  • 0 kudos

Is there more technical info on the ISPU available?

I would like to use the ISPU on the LSM6DSO16ISTR for signal processing of both the internal and a few external sensors. I'm having trouble finding any details on the ISPU itself. How about:Instruction set architecture Register fileBoot loaderClockin...

MFlam.1 by Associate
  • 1107 Views
  • 0 replies
  • 2 kudos

Resolved! LIS2DH12TR / LIS3DHTR

Is LIS2DH12TR / LIS3DHTR a 10-year commitment? How long does it live?

xwang.6 by Associate III
  • 1534 Views
  • 1 replies
  • 0 kudos

LSM6DSL - Temperature Accuracy

We have several units of LSM6DSL in the field and I was looking that this part has an embedded temperature sensor. I would like to understand better the accuracy of this sensor. The datasheet is not clear, showing only this information. Can I assume ...

0693W00000aJ3JmQAK.png 0693W00000aJ3L9QAK.png
RNJ by Associate II
  • 1582 Views
  • 1 replies
  • 0 kudos

From Unico to Real Application

Hello,I plan to use STEVAL-MKI109V3 with LSM6DSV16x. Assumed that I used Unico and collected data, and labelled them. How can I use my custom training in different MCU?Also, I need wireless communication instead of a USB Cable to collect my data. How...

FKara.3 by Senior
  • 1160 Views
  • 1 replies
  • 0 kudos

Resolved! SPI mode on the steval-mki227ka

On the website, in the databrief it is not stated how to connect the jumpers on the steval-mki227ka, I would like to know how to enable SPI mode 1 on the evaluation kit for testing.The problem that I'm getting is that even reading the who am I addres...

KRudo.1 by Associate
  • 2546 Views
  • 3 replies
  • 0 kudos

Resolved! Change ODR on SensorTile

Hello,I programmed the sensorTile STEVAL-STLKT0V1 with ALLMEMS1 end I used STM32CubeIDE with NUCLEO32. How I can change the sampling frequency (ODR) of accelerometers and gyroscopes?Thanks,Chiara

CRoma.11 by Associate II
  • 6330 Views
  • 12 replies
  • 0 kudos

User calibration for LSM6DSM IMU?

I'm designing production test for a board that integrates the LSM6DSM imu. I was wondering if it was necessary to do any calibration of the IMU during the test process or if the factory calibration is sufficient?

PCher.4 by Associate
  • 1380 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.