2021-02-25 9:35 AM
Hello,
Is there any reason which could explain I cannot connect to the sensor using GATT interface on Windows ?
The sensor often return, file not found, aborted or it is not able at all to connect to the sensor.
Application of ST in IOS works. Custom application with accelerometer has been pushed.
The only difference I have if I compare with another sensor which is working, it is the passcode.
Regards,
2021-03-04 12:01 AM
I found the ALLmEMSensor1 which seems to send gyro, avec, magn in 1 characteristic.
Another question, i was able to send data to Azure IoT central App but not to Azure IOT Hub. Is it possible ? URI of connection is not recognized, but maybe i do not use the correct one.
2021-03-04 4:19 AM
Hi @ACout.1 ,
very good for the single char, I did not remember that that fw had a single one for the motion sensors.
Regarding the Azure issue, the SensorTile.box is not configured to work with the Azure IOT Hub, only with the central app, so the outcome is normal.
Niccolò
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.