cancel
Showing results for 
Search instead for 
Did you mean: 

Questions about the maximum absolute ratings of ASM330LHH

ggob
Associate III

I have a question regarding the absolute maximum ratings of the ASM330LHH.

In the datasheet, the Vin rating lists “(including CS, SCL/SPC, SDA/SDI/SDO, SDO/SA0)”.
Does this voltage range also include any overshoot and undershoot on these pins?

Additionally, if overshoot or undershoot exceeds the absolute maximum ratings,
what potential issues could occur (e.g., malfunction, degradation, or damage to internal circuitry)?

 

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

The answer to this question is universal, i.e. it applies to each and every device:

If the values specified in the Absolute Maximum Ratings table are exceeded, the function of the device can no longer be guaranteed. It is impossible to define the potential consequences of exceeding these values. It is the responsibility of the respective developer to comply with the Absolute Maximum Ratings by using suitable protective measures, e.g. Transient voltage suppressors (TVS).

Does it answer your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

The answer to this question is universal, i.e. it applies to each and every device:

If the values specified in the Absolute Maximum Ratings table are exceeded, the function of the device can no longer be guaranteed. It is impossible to define the potential consequences of exceeding these values. It is the responsibility of the respective developer to comply with the Absolute Maximum Ratings by using suitable protective measures, e.g. Transient voltage suppressors (TVS).

Does it answer your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.