cancel
Showing results for 
Search instead for 
Did you mean: 

LSM9DS0 debugging

sasha_hurovitz
Associate
Posted on July 11, 2016 at 22:52

Hi all,

I've recently bought a couple of LSM9DS0's for a simple project.

Before soldering them to my board I tried to checked if everything was right.

I ONLY connected pin 5 and 6 to GND and 15, 16 and 17 to 3v3.

However when I turned on the power supply, it showed up a short circuit.

I was wondering if anyone has an idea on what is wrong.

I don't think that I burnt them by static as I used them with a wrist band connected to GND.

Besides, the cut-off current on the power supply is set to 200mA.

I'm also attaching the design of the board I was planning to use with the IMU if anyone has an opinion about it.

Best regards
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.