2016-05-04 7:07 AM
Hi to all, i have this shield x-nucleo-6180XA1 with mi STM32L152RE, i setting PB8 and PB9 for I2C1, i want to test the shild i want to see the who i am, i write this easy code
&sharpdefine IDENTIFICATION__MODEL_ID 0x000 //who I am &sharpdefine PROXW 0x52 &sharpdefine PROXR 0x53 &sharpdefine DEFUALT_ADDR 0X29 void I2C_WHOAMI(I2C_HandleTypeDef *hi2c1, __IO uint8_t whoami){ while((hi2c1->Instance->SR2&BUSY)==BUSY); // Start hi2c1->Instance->CR1 |= START; while((hi2c1->Instance->SR1&SB)!=SB); dummy16 = hi2c1->Instance->SR1; hi2c1->Instance->DR = PROXW; while((hi2c1->Instance->SR1&ADDR)!=ADDR); dummy16 = hi2c1->Instance->SR1; dummy16 = hi2c1->Instance->SR2; while((hi2c1->Instance->SR1&TXE)!=TXE); hi2c1->Instance->DR = whoami; //WHOAMI; while((hi2c1->Instance->SR1&(TXE|BTF))!=(TXE|BTF)); // Restart hi2c1->Instance->CR1 |= START; while((hi2c1->Instance->SR1&SB)!=SB); dummy16 = hi2c1->Instance->SR1; hi2c1->Instance->DR = PROXR; while((hi2c1->Instance->SR1&ADDR)!=ADDR); dummy16 = hi2c1->Instance->SR1; dummy16 = hi2c1->Instance->SR2; while((hi2c1->Instance->SR1&(RXNE))!=(RXNE)); dummy16 = hi2c1->Instance->DR; if (dummy16==(uint16_t)180) //0xB4 { HAL_GPIO_WritePin(LD2_GPIO_Port,LD2_Pin,GPIO_PIN_SET); while((1)); } hi2c1->Instance->CR1 |= STOP; } in the main.c i have this // whoami I2C_WHOAMI(&hi2c1,IDENTIFICATION__MODEL_ID); i don't see nothing, i use this code with other shield it's work well. can you help me? best regards A. #nucleo #x-nucleo #i2c2016-05-04 7:55 AM
2016-07-11 4:52 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.