2022-09-09 2:26 AM
The datasheet for the LSM6DSO does not specify the tolerance of the linear acceleration sensitivity. Can you please tell me what the linear acceleration sensitivity tolerance is for this part.
To be clear, I would expect to find offset and sensitivity accuracy/tolerance figures for linear acceleration and angular velocity:
* LA_TyOff: Linear Acceleration offset accuracy
* LA_So%: Linear Acceleration sensitivity tolerance
* G_TyOff: Angular Velocity offset accuracy
* G_So%: Angular Velocity sensitivity tolerance
The datasheet has three of these (LA_TyOff, G_TyOff and G_So%), but is missing LA_So%.
2022-09-13 7:23 AM
Hi @Community member ,
from characterization data, I can indicate you +-1% / +-2% as typical value for the LA_So% parameter.
-Eleon
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.