2014-07-07 6:40 AM
Hi all,
I am working with the LSM303C and with the EVALBoard ST8S003VLDISCO.
When i want to access the Magnetometer data it is giving me some strange values.The Values of the High-Byte are staying constant always with the same values while the Low-Bytes are jittering a lot - not reacting to an external magnet.
I can say that the I2C is working properly, because i am able to read and write registers.
The Sensor is also working. I`ve tested it with another system.I tried several configurations that work with an Arduino and M3 Board from NI - but it doesnt work.
Do you know what this could be?
The Accelerometer works properlyRegards
AscheWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.