2014-06-25 10:39 AM
Bought this eval board.
Hooked it up to a TI Launchpad... I run the SPI in 4 wire... I can see the SPI buss sending data (o-scope)...timing good, clocks good, setup good... When I READ I see the data coming back BEFORE the 8th clock cycle...???? Almost like something is ''jacked'' inside the device... for a test, I step back and forth from writing to a CNTRL reg and then reading it back... (i.e. send 0x00 to CNTRL0 (reg 0x1F)..then I read it back...I see 0 read back...then I increment the data (write 0x01 to CNTRL0)..read it back...I see the ''1'' come back on the 8th clock...not the sixteenth (on a read: R/W=1, MS=0, A5-A0...dummy data for 8 bits...the data from SDO should come back on those last 8 clk's....correct?) so what am I missing?... I also unhooked the SDO from the TIVA (in case of some prob there)...same deal.... bad part?...bum eval kit?..... bueller...bueller....anyone?..... send me email jyoung AT lauferwind DOT com #lsm303dWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.