2017-07-16 11:22 PM
hello,
I have gone through the datasheet and app note of LIS3MDL. But i am not able to get how block data update bit work i.e. if someone has set the BDU bit and if I read registers through I2C one by one, then how the ic internally gets idea that all the registers have been read and got the data of same sample?
Also can anyone please elaborate about ODR and its working in LIS3MDL
Solved! Go to Solution.
2017-07-17 9:53 AM
Hello,
Have a look at this application note, available from product webpage:
. Section 3.2.3 Using the block data update (BDU) feature explains the BDU.Also ODR is output data rate, how often you can get an updated results. It is declared in Hz, meaning samples per second.
David
2017-07-17 9:53 AM
Hello,
Have a look at this application note, available from product webpage:
. Section 3.2.3 Using the block data update (BDU) feature explains the BDU.Also ODR is output data rate, how often you can get an updated results. It is declared in Hz, meaning samples per second.
David
2017-07-18 1:01 AM
Yes, your understanding is correct.
2017-07-18 2:16 AM
Hello David,
Thanks for your reply.
But still i am not getting full idea about ODR. So i just want to confirm from you that my understanding is right or not from your answer.
So what i have understood is, by setting ODR=80Hz, our output registers will be updated every 12.5ms(1/80). Is it right?
2017-07-18 3:24 AM
Thank You Miroslav for your help.
2017-07-18 5:58 AM
Hello,
if i set full scale to +-4 gauss, then can we measure the magnetic field greater then 4 gauss and lesser then -4 gauss?
I am not able to understand FullScale parameter from datasheet of LIS3MDL. So can you please help me to understand it
2017-07-18 6:17 AM
Hello, have a look at section Mechanical characteristics in the datasheet. Each scale has a defined sensitivity per LSB. After you read the output registers, multiply the value by the sensitivity and you get you reading in mg units.
2017-07-18 7:11 AM
Hello David,
Thanks for your reply.
Actually I know that thing ,but i want to know that, do full scale define measurement range? which means setting +-4 Gauss in Full Scale, can we measure the magnetic field beyond 4 gauss?
2017-07-18 8:00 AM
Yes, full scale is basically measurement range. For example for Full Scale +-4 Gauss you can measure magnetic field from -4 Gauss to +4 Gauss.
Even if values higher than 4 Gauss (or lower than -4 Gauss) can fit in the output register's range the functionality and performance is not guaranteed.
2017-07-19 7:07 AM
Hi Miroslav,
Thank you for your response. It cleared my doubt fully.
Another thing that i want to confirm is, if i set some value in OFFSET registers, does it internally subtract the OFFSET values and writes the output in OUT registers, or we have to do it manually.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.