2025-06-30 12:25 AM - last edited on 2025-06-30 6:44 AM by mƎALLEm
Hello,
I’m working with the LIS2DW12 vibration sensor for single-tap detection. I have configured the sensor registers according to the application note for enabling single tap.
When I continuously read the TAP_SRC register in polling mode, I’m able to detect single taps successfully.
However, I want to use interrupts instead of polling. I have connected the LIS2DW12’s INT1 pin to the PE7 GPIO pin of my STM32L496 controller. Despite this, I am not receiving any interrupt signal on PE7 when I tap the sensor. please check the single tap init function :
void LIS2DW12_Init_Single_TAP(void) {
message[0] = 0x74;
if(HAL_I2C_Mem_Write(&hi2c3, LIS2DW12_Adrr, CTRL1, 1, message, 1, 1000)==HAL_OK)
{
message[0] = 0x0C;
if(HAL_I2C_Mem_Write(&hi2c3, LIS2DW12_Adrr, CTRL6, 1, message, 1, 1000)==HAL_OK)
{
message[0] = 0x09;
if(HAL_I2C_Mem_Write(&hi2c3, LIS2DW12_Adrr, TAP_THS_X, 1, message, 1, 1000)==HAL_OK)
{
message[0] = 0xE9;
if(HAL_I2C_Mem_Write(&hi2c3, LIS2DW12_Adrr, TAP_THS_Y, 1, message, 1, 1000)==HAL_OK)
{
message[0] = 0xE9;
if(HAL_I2C_Mem_Write(&hi2c3, LIS2DW12_Adrr, TAP_THS_Z, 1, message, 1, 1000)==HAL_OK)
{
message[0] = 0x06;
if(HAL_I2C_Mem_Write(&hi2c3, LIS2DW12_Adrr, INT_DUR, 1, message, 1, 1000)==HAL_OK)
{
message[0] = 0x00;
if(HAL_I2C_Mem_Write(&hi2c3, LIS2DW12_Adrr, WAKE_UP_THS, 1, message, 1, 1000)==HAL_OK)
{
message[0] = 0x40;
if(HAL_I2C_Mem_Write(&hi2c3, LIS2DW12_Adrr, CTRL4_INT1_PAD_CTRL, 1, message, 1,1000)==HAL_OK)
{
message[0] = 0x00;
if(HAL_I2C_Mem_Write(&hi2c3, LIS2DW12_Adrr, CTRL3, 1, message, 1, 1000)==HAL_OK)
{
HAL_Delay(10);
message[0] = 0x22;
if(HAL_I2C_Mem_Write(&hi2c3, LIS2DW12_Adrr, CTRL7, 1, message, 1, 1000)==HAL_OK)
{
printf("\r\n single tap init completed!\r\n");
}
}
}
}
}
}
}
}
}
}
}
this is the gpio callback for interrupt:
void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin){
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_10, GPIO_PIN_SET); // HeartBeatLed
if (GPIO_Pin == GPIO_PIN_7) {
uint8_t tap_src=0;
HAL_I2C_Mem_Read(&hi2c3, LIS2DW12_Adrr, 0x39, 1, &tap_src, 1, 1000); // Read TAP_SRC
if (tap_src & 0x40) { // TAP_IA bit
tap_detected = 1;
// HAL_GPIO_WritePin(GPIOD, GPIO_PIN_10, GPIO_PIN_SET); // HeartBeatLed
}
}
}
IRQ handler:
void EXTI9_5_IRQHandler(void)
{
/* USER CODE BEGIN EXTI9_5_IRQn 0 */
/* USER CODE END EXTI9_5_IRQn 0 */
HAL_GPIO_EXTI_IRQHandler(INT1_IMU_Pin);
/* USER CODE BEGIN EXTI9_5_IRQn 1 */
/* USER CODE END EXTI9_5_IRQn 1 */
}Could you please help me with:
Sensor Configuration: Are there any additional registers I should configure to properly route the single-tap interrupt to INT1?
STM32 GPIO Setup: Are there any specific settings needed on PE7 (e.g. interrupt mode, pull-up/pull-down, EXTI configuration) to detect the interrupt?
Troubleshooting Tips: How can I confirm whether the sensor is actually toggling the INT1 pin during a tap event?
Thanks in advance for your support!
2025-06-30 7:57 AM
I checked the interrupt signal for the single-tap feature using a Picoscope, but no signal is appearing. The interrupt triggers only very rarely—about four times in an entire day. I currently don’t have any other solutions to resolve this issue. Could you please help me with a solution or share any reference code if available?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.