2020-02-12 6:16 AM
hi,
i'm trying to read x,y,z values using FIFO - LIS2DE12_FIFO_READ_START
but every time get zero in all the answers, also try to read separately x,y,z
in the address LIS2DE12_OUT_X_H,LIS2DE12_OUT_Y_H,LIS2DE12_OUT_Z_H
in this mode I'm getting values but always the same values - the numbers dont changes
(I used the driver from this link in the same configuration -
https://github.com/STMicroelectronics/STMems_Standard_C_drivers/tree/master/lis2de12_STdC , read_data_simple.c) - this don't work
in addition the who-iam check is working.
Thanks,
Maor
2020-02-12 6:49 AM
I had a similar effect with the MKI137 (LIS3MDL sensor) and the Unico application.
I only got consistent sensor values other then zero once I set the sensor to a run-mode from the GUI. Default was Low Power mode (CTRL_REGs 1 & 4 for the LIS3).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.