2022-10-04 4:51 AM
Solved! Go to Solution.
2022-10-05 2:15 AM
Table 3 of the data sheet confirms the width of the measuring value with 12bit = 0...2047.
For example, with FS1,FS0=0b01 in CTRL-REG4 the measuring range FS is set to 200g, the sensitivity So is 98mg/digit, resulting in a necessary number of values of 200'000/98 = 2040.8. For this 12bit are exactly sufficient, ditto for the other measuring ranges.
As @Community member mentioned, the 16bit data results from the necessity that the higher-level controller typically wants to have multiples of bytes. Nevertheless, only 12 bits of significant data are contained in this 16-bit data packet for the measured value.
Is that a little clearer now?
Regards
/Peter
2022-10-04 5:11 AM
12 isn't a multiple of 8, whereas 16 is
2022-10-04 11:10 PM
True, still this doesn't mean anything... did you take a look on page 9, section sensitivity, of the datasheet? that's why I am confused... there it says 12-bit representation
2022-10-05 2:15 AM
Table 3 of the data sheet confirms the width of the measuring value with 12bit = 0...2047.
For example, with FS1,FS0=0b01 in CTRL-REG4 the measuring range FS is set to 200g, the sensitivity So is 98mg/digit, resulting in a necessary number of values of 200'000/98 = 2040.8. For this 12bit are exactly sufficient, ditto for the other measuring ranges.
As @Community member mentioned, the 16bit data results from the necessity that the higher-level controller typically wants to have multiples of bytes. Nevertheless, only 12 bits of significant data are contained in this 16-bit data packet for the measured value.
Is that a little clearer now?
Regards
/Peter
2022-10-06 12:59 AM
Hi Peter!
Thanks a lot for your answer! So, the 12 less significant bits of the output data do always contain the full information, right?
2022-10-06 1:54 AM
to be honest, the results I get make more sense if I consider all 16Bits to be valid... that would mean for range FS = 200g -> 6,1 mg/digit ((2*200g*1000)/(2^16-1) digit)...are you sure that table3 on page 9 is correct?
2022-10-06 2:15 AM
Well, you could call it centred, because the measured values are output in two's complement.
Yes, table 3 is correct and refers to the actual measurement result.
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.