2021-08-10 2:32 AM
2021-09-01 5:06 AM
Hi @Snara.2 ,
may I ask you to clarify this answer:
[I have installed ST link. If I use STEVAL-STLK01V1 Kit I shall able to see the Virtual UART and if I conenct STEVAL-MKSBOX1V1 and used BLE Sensor from the functional pack and enabled the # define for USART2]
2021-09-01 9:12 AM
@niccolo.ruffini I have downloaded two different functional packs available for both the development boards. The functional pack which comes along with the STEVAL-MKSBOX1 is not working. The attached project (BLE_1DeviceName) is the one newly created to check the advertisement and later on validate the customer service and characteristics.
2021-09-02 12:22 AM
2021-09-02 7:04 AM
I have enclosed the BLE_DeviceName Project which is created for STEVAL - MKSBOX1V1 and XCUBE -BLE2 software package. I have two issues one is non detection of USB debugging and other one is BLE code is not working...
Is it possible to check and guide me what is the issue. I have included only Device Name in the BLE code,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.