2019-12-10 7:55 AM
I used the breakout and evaluation board with Unico.
Now I want to use my own board with sensor.
I want to use Unico to capture, process, display sensor data.
I may need to implement the communication protocol via serial port.
Do you have some documents about how to do it? Thanks
2019-12-10 9:04 AM
Hi @CLI.2455 , not so simple to interface a custom board with Unico-GUI... you should at least use the same MCU of the to STEVAL-MKI109V3 and a similar schematic in order to be able to upload the proper firmware (which is however not open) and make the Unico-GUI compatible with the hardware platform. Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.