2022-07-01 7:59 AM
We've designed the LSM6DSO32X (using I2C interface) into a system and would like to use the STEVAL-MKI109V3 tool and UNICO-GUI to test and program the machine learning algorithms. Scoping the STEVAL-MKI109V3/STEVAL-MKI221V1 combination, I find that UNICO-GUI is using I2C address 0x6B for the LSM6DSO32X, but of course in our design with configured it at 0x6A. Is there a (hopefully easy) way to configure UNICO-GUI to talk to an LSM6DSO32X at I2C address 0x6A?
2022-07-05 8:22 AM
Hi @Brian Rau ,
Unfortunately, there is no way to set the I2C address from Unico-GUI. I2C address is set from the STEVAL-MKI109V3 firmware to work with the respective adapter board.
If you are using a “STEVAL-MKI109V3/STEVAL-MKI221V1 combination�? as you wrote, you should not have problems in using Unico with ST hardware, without changing the I2C address.
On the other hand, if you are using a custom hardware, then you could:
-Eleon
2022-07-05 12:21 PM
Is the STEVAL-MKI109V3 firmware source available anywhere to modify the I2C address used?
2022-07-06 3:44 AM
Hi @Brian Rau ,
no, unfortunately the source code of STEVAL-MKI109V3 is not publicly available.
-Eleon
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.