2024-01-17 12:58 AM
Hi All,
I started with example to make STHS34PF80 presence detection working.
Now I tried to add effective presence detection range.
Where should I start ? Is there a suggested process ?
2024-01-18 12:22 AM
2024-01-18 12:57 AM
My existing code is based on this example, however the presence detection range is around 1.2 meters.
I want to extend the range up to 2.5~3 meters however there is no criteria in example what parameters to tune.
2024-02-01 5:31 AM
Hi @SLin.11 ,
You can detect the presence at higher distance changing the threshold. Keep in mind that the sensor must be tuned based on the application and the environmental conditions.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.