2022-08-08 2:34 AM
Hi Everyone,
I am using STEVAL-MKI182V2 IMU sensor and can able to get the Euler angles of Yaw=360 degrees , Pitch= +- 180 degrees and Roll=+-90 degrees, now i want to get the Roll with range of +- 60 deg how can i get that range, please suggest me.
Thank you.
2022-08-08 3:14 AM
The roll angle in degree is a physical property of the sensor pose. What do you want to limit here?
hth
KnarfB
2022-08-08 9:24 PM
Hi KnarfB,
I want to limit the angle of rotation for Roll axis to +- 60 degrees instead of +-90 degrees
2022-08-12 5:52 AM
Hi @Anil ,
I'm not sure I have caught the point... If you want to limit a rotation angle, you should act clamping your system at physical level, while if you want to convert a 0deg-90deg angle linearly into a 0deg-60deg angle you should do the relative proportion.
-Eleon
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.