Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
I have some questions regarding loading machine learning core configurations, specifically onto the lsm6dsox chip but it should be the same across devices. I have generated .ucf and .h files. I've confirmed that the .ucf file works fine when loaded w...
Hi there fellas, i got me two Steval-Stwincsv1 and i'm now using the HSDataLog. Everything works perfectly when only one of the sensors is plugged on to the Computer. When i plug the second one and start it, one of them start, and ONLY ONE. It seems ...
Hi Everyone,I am using STEVAL-MKI182V2 IMU sensor and can able to get the Euler angles of Yaw=360 degrees , Pitch= +- 180 degrees and Roll=+-90 degrees, now i want to get the Roll with range of +- 60 deg how can i get that range, please suggest me.T...
If the ISM330DLC is connected to two separate dedicated SPI buses (i.e. no other SPI slaves on the bus) can the CS and OCS_Aux pins be connected to ground or do they have to be controlled by their respective SPI masters?
hello.I am using LSM6DSM to collect acceleration and gyro data.Data is being collected at 52Hz using FIFO, but the actual data collected is about 51.2Hz.It is probably caused by the LSM6DSM internal clock being inaccurate. Is there a way to correct t...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.