cancel
Showing results for 
Search instead for 
Did you mean: 

Does the STEVAL-MKI109V3 have onboard support for sensor fusion using the STEVAL-MKI159V1?

DCorl.2
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Eleon BORLINI
ST Employee

Hi @DCorl.2​ ,

the library implementing the sensor fusion with ST sensors is the MotionFX, and it is not so straightforward to be used with STEVAL-MKI109V3, since its FW is not open-source.

The suggestion of the UM2220 user manual is to run this implementation of the sensor fusion here:

The software comes with sample implementation running on an X-NUCLEO-IKS01A2, X-NUCLEO-IKS01A3 or X-NUCLEOIKS02A1 expansion board on a NUCLEO-F401RE, NUCLEO-L476RG, NUCLEO-L152RE or NUCLEO-L073RZ development board.

But of course you can configure all the device registers with the STEVAL-MKI109V3 + Unico-GUI.

-Eleon

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.