2021-12-01 1:42 AM
Solved! Go to Solution.
2021-12-01 1:43 AM
Absolutely yes, ST offers on GitHub not only the configuration files which can be used to program the sensor for a quick start, but also configuration details (in the README file), and examples of dataset which can be used to generate the final configuration. The configuration can be fine-tuned using new datasets or different MLC parameters.
2021-12-01 1:43 AM
Absolutely yes, ST offers on GitHub not only the configuration files which can be used to program the sensor for a quick start, but also configuration details (in the README file), and examples of dataset which can be used to generate the final configuration. The configuration can be fine-tuned using new datasets or different MLC parameters.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.