cancel
Showing results for 
Search instead for 
Did you mean: 

Acitivity/Inactivity duration configuration

RK1803
Associate

I am working with LIS2DW12 configuring the INT1 for the activity/inactivity interrupt. With the below configurations (as provided in the datasheet), 

1. Write 50h in CTRL1 // Turn on the accelerometer // ODR = 200 Hz, FS = ±2 g

2. Write 42h in WAKE_UP_DUR // Set duration for inactivity detection // Set duration for wake-up detection

3. Write 42h in WAKE_UP_THS // Set activity/inactivity threshold // Enable activity/inactivity detection

4. Write 20h in CTRL4_INT1_PAD_CTRL // Activity (wake-up) interrupt driven to INT1 pin

5. Write 20h in CTRL7 // Enable interrupts

As expected the interrupt is triggered as an when there is an activity (movement).

I want the interrupt to be triggered when the activity is prolonged for 5 secs. I tried playing around with the CTRL1 & WAKE_UP_DUR settings. But results are not as expect. Kindly advice.

 

 

 

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
Federica Bossi
ST Employee

Hi @RK1803 ,

The wake-up interrupt event can be delayed in function of the value of the WU_DUR[1:0] bits of the WAKE_UP_DUR register: 1 LSB corresponds to 1/ODR time, where ODR is the accelerometer output data rate.

When the wake-up event is detected, the interrupt is set high for 1/ODR period, then it is automatically deasserted
(the WU_IA event on the pin must be routed by setting the INT1_WU bit of CTRL4_INT1_PAD_CTRL register
to 1).

To achieve the desired wake-up interrupt delay on the LIS2DW12, it is essential to correctly configure both the WAKE_UP_DUR register value and the Output Data Rate (ODR), considering that the delay equals WAKE_UP_DUR × (1/ODR) × a multiplier defined by the WU_DUR[1:0] bits.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Federica Bossi
ST Employee

Hi @RK1803 ,

The wake-up interrupt event can be delayed in function of the value of the WU_DUR[1:0] bits of the WAKE_UP_DUR register: 1 LSB corresponds to 1/ODR time, where ODR is the accelerometer output data rate.

When the wake-up event is detected, the interrupt is set high for 1/ODR period, then it is automatically deasserted
(the WU_IA event on the pin must be routed by setting the INT1_WU bit of CTRL4_INT1_PAD_CTRL register
to 1).

To achieve the desired wake-up interrupt delay on the LIS2DW12, it is essential to correctly configure both the WAKE_UP_DUR register value and the Output Data Rate (ODR), considering that the delay equals WAKE_UP_DUR × (1/ODR) × a multiplier defined by the WU_DUR[1:0] bits.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.