2024-06-04 2:37 PM
Further to this earlier post, any chance now is a BMA400 SPI library already ported to STM32CubeIDE?
Many thanks
Solved! Go to Solution.
2024-06-05 6:42 AM
Well, STM32CubeMX generates standard C and the STM32CubeIDE can also work with it. The HAL was also created in standard C.
So why not just use the library?
2024-06-04 11:16 PM
What's stopping you from using the GitHub library that @Foued_KH mentioned there?
Regards
/Peter
2024-06-05 6:21 AM
That time-ago message is in 'standard c'. As time has gone by, we are enquiring if someone has happen to know a version that has been adopted into STM32CubeIDE MX and HAL format.
Many thanks
2024-06-05 6:40 AM
If it's "Standard C", then it will be acceptable to any C IDE!
2024-06-05 6:42 AM
Well, STM32CubeMX generates standard C and the STM32CubeIDE can also work with it. The HAL was also created in standard C.
So why not just use the library?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.