2013-12-13 10:45 AM
If the LIS3DH range is set to +/- 2g, how does the chip behave if acceleration exceeds 2g's? Do the axis outputs limit, wrap around, go to some fixed value, etc?
2014-01-10 5:21 AM
Hello Charles,
the output value will show the maximum value allowed by that full scale. In this case, for 2g, if you apply a 4g acceleration, the output will show the maximum of 2g. Thank you, Thiago ReisWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.