MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LPS27HHTW guidelines for system integration

Hello everyone, I'm looking for an application note (similar to AN5063 but for the LPS27HHTW sensor) to get an idea of the mechanical integration and any necessary tolerances. Additionally, I wanted to ask the community if anyone has installed two se...

LuigiG by Associate
  • 1273 Views
  • 1 replies
  • 2 kudos

LIS2D12

I use LIS2DS12 This is my init function   void LIS2DS12_Init(void) { uint8_t ctrl_1 = 0x72; //0111 for 6.4kHz ODR [7:4], 00 for 2g [3:2], 1 for high frequency available[1], 0 for BDU not activated [0] uint8_t ctrl_2; // [6] for soft_reset, [1] for ...

fru999_0-1719563774185.png fru999_1-1719563790647.png
fru999 by Associate III
  • 10354 Views
  • 27 replies
  • 3 kudos

Resolved! Common SPI - LPS22HB pressure/temp sensor

Dear ST technical support.Please can you advise the pin configuration and bus timing (period between active devices) to allow me to connect three of your LPS22HB pressure sensors in parallel on the same SPI bus?The CS pin is used to enable the SPI fu...

DuncanR by Associate II
  • 4498 Views
  • 6 replies
  • 1 kudos

LIS3MDL: unexpected readings

Posted on June 05, 2017 at 20:31Hi,We're using LIS3MDL to detect changes in the earth magnetic field due to various metallic objects flowing in the sensor proximity. So, we are not interested in the correctness of the absolute values in order to pro...

LIS3MDL - Problem with readings after calibration.

We embed lis3mdl on our board that we produce, most of them are perfect, unfortunately there are single pieces where the magnetic north is wrong, the heading is wrong by up to 60-100 degrees. What could be the reason ? Regards. 

TBart.1 by Associate II
  • 5016 Views
  • 8 replies
  • 1 kudos

I have a problem of power down of ASM330LHH

As you can see, I was doing a test where I tried setting the gyroscope and accelerometer to power down mode and gave it a 10ms delay, which I called time 1, while I again turned the gyroscope on The accelerometer is set to high-performance mode, and ...

2.png

Issues with 3 LSM6DSV16X on the same SPI bus

Hello, I am trying to interface a TI MCU with three LSM6DSV16X sensors using SPI communication on the same bus. My setup consists of 3 chip select lines with a 10 kΩ pull-up resistor (on all sensor boards), POCI (MISO) with a single 10 kΩ pull-up res...

Nico5 by Associate
  • 3837 Views
  • 4 replies
  • 0 kudos

ISM330DHCX GDA only set once

I have an application using the XL function, it works fine, no issues.Now I need to read the gyroscope output data.After I finish configuring the registers:CTRL9_XL 01INT1_CTRL 03INT2_CTRL 06CTRL1_XL 30CTRL2_G 32CTRL3_C 04CTRL6_C 80CTRL8_XL 00MD1_CFG...

Claude by Associate III
  • 1675 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.