MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

IIS2DH Reading FIFO

Posted on April 13, 2017 at 01:08With a 2g scale sampling @25Hz the FIFO fills with data and I am reading the contents up to the watermark. HR and LPen are disabled.With the Z-Axis pointing toward earth I get the following data for the X-Axis using ...

LSM303DLHC DRDY Behaviour

Posted on April 13, 2017 at 12:58The detailed behaviour of the LSM303DLHC DRDY pin (pin 9) is not elaborated upon in the datasheet.We have observed that it generates active low pulse but this is not detailed in the datasheet. What are the timing req...

tom2399 by Associate
  • 967 Views
  • 1 replies
  • 0 kudos

IIS2DH Reading and Clearing FIFO

Posted on April 12, 2017 at 17:13I am moving to the IIS2DH from the LIS3DSH because it is end of life. I am having an issue with reading the FIFO. I can enable FIFO mode and it seems to fill and generate an interrupt on OVRN and WTM just fine, but t...

Magnetometer difference between LSM9DS0 and LSM9DS1

Posted on April 11, 2017 at 08:08 We are upgrading our IMU from a LSM9DS0 to LSM9DS1. However we are having issues with the magnetometer on the LSM9DS1. Even after min/max calibration it doesn't appear to give correct heading. We are aware tha...

LIS3MDL SPI BUS Problem

Posted on April 11, 2017 at 12:31Hi, I have designed a circuit which has 8 LIS3mdl sensor slot on 1 spi bus.The problem when I connect only one ls3mdl sensor (other 7 are empty) to the board it works well. but most of the when I connect another one ...

Sadra nsh by Associate II
  • 2048 Views
  • 3 replies
  • 0 kudos

LIS2DHTR Reflow Issue

Posted on March 30, 2017 at 21:02Hello,     We are working with the LIS2DHTR and have had significant yield issues after running the board through the reflow oven.  For the next run we plan to lower the temperature.  But for now we are replacing the...

LSM6DSL Min/Max specifications for ODR (Output Data Rate)

Posted on March 21, 2017 at 15:35I'm using the LSD6DSL in an application where the sampling rate (ODR for the MEMs) is important. The ODR in the datasheet is only given as 'Typical'. Could I get a more precise specification for the ODR, e.g. min/max...

cn2 by Associate II
  • 977 Views
  • 1 replies
  • 0 kudos

use X-NUCLEO-53L0A1 satellites as proximity sensor

Posted on March 29, 2017 at 08:37Hi, I'm new with stm32 and mbed environment. I'm trying to use VL53L0X satellites as proximity/distance sensor but I have few unsolved questions: 1) in this datasheet I can see that only first six pin of satellites a...

www.st.com

Posted on April 03, 2017 at 12:56Apple watch accelerometer axis range Hi good morning,I'm developing an apple watch health care application. After a search i discover an ST microelectronics accelerometer sensor mounted on a system on a chip internal...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.