2017-03-21 7:35 AM
I'm using the LSD6DSL in an application where the sampling rate (ODR for the MEMs) is important. The ODR in the datasheet is only given as 'Typical'. Could I get a more precise specification for the ODR, e.g. min/max values over the entire temperature range. I suppose this ODR is generated from an internal oscillator with tolerance, temperature drift, ...
2017-04-09 12:02 AM
Unfortunately this information cannot be shared on ST Community web.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.