MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS3DH spike in acceleration value

Posted on April 10, 2018 at 17:13I have been doing some testings recently with the LIS3DH accelerometer to measure machine vibration, and I have come across 2 things. I am using the accelerometer to sample 512 points at a 1.1Khz sampling rate. I hav...

0690X0000060AWLQA2.png

Battery life STEVAL-STLKT01V1 SensorTile

Posted on April 04, 2018 at 12:09Hi, I have the sensortile development kit, I wanted to test the battery life without soldering the sensortile to the cradle board, without using USB charge and with the accelerometer always active. Does anyone who ha...

VL6180X ECE threshold calculation

Posted on April 10, 2018 at 20:41Trying to figure out how to apply the Early Convergence Estimate value for the VL6180X proximity sensor.Design Tip DT0034 gives some information, but also populates the equations with some apparent magic numbers, and...

LSM303AGR with switchend GND

Posted on March 29, 2018 at 13:03Hi thereI'm developing an ultra-low-power minituarized system witch includes the LSM303AGR. since the power comes only from a small battery, the sleep-current of the LSM303AGR is too high, therefore we want to power ...

The LIS3DH crash test reads an abnormal acceleration value

Posted on April 10, 2018 at 04:14     When I was doing impact testing, using the 16g range, with my device gently knock on the desktop, the acceleration values read have acceleration values of more than 10g, a bit unbelievable, acceleration reading ...

0690X00000604NOQAY.jpg
? ?_3 by Associate II
  • 1307 Views
  • 1 replies
  • 0 kudos

Resolved! Questions about the interrupt config for Lis3dx

Posted on April 08, 2018 at 08:261) CTRL_REG3 (22h)Can I set both I1_IA1 and I1_IA2? 2) What is I1_321DA? 3) Our project uses two threshold, one for stronger force (e.g. collision), the other for weaker force (e.g. impact). I assume I should set INT...

0690X0000060ASxQAM.png 0690X0000060APaQAM.png 0690X0000060ATHQA2.png
Kefei Yao by Associate III
  • 2122 Views
  • 3 replies
  • 1 kudos

Resolved! Can't get IG2 work on either INT1 or INT2 for Lis3de

Posted on April 08, 2018 at 13:13I encountered a problem that IG2 doesn't get detected on either INT1 or INT2 pin. I confirm the IG1 work on both INT1 and INT2. Followings are the combinations I tried (CTRL REG1,2,4,5 kept unchanged):The INTx_CFG,IN...

Kefei Yao by Associate III
  • 1220 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.