MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Cann't complie to eMotionV2_REL_5.0.0.zip(in en.stsw-mki109w.zip)?

Posted on April 24, 2018 at 10:20Hi..i use steval-mki1092V2(demo board) with mki160V1(sensor)..so i was download to en.stsw-mki109w.zip(for Windows) file...and  i use to IAR Embeded Work...7.20 Version...so when i open project file,come to msg like ...

sw lee by Associate II
  • 832 Views
  • 0 replies
  • 0 kudos

LPS33HW - false reading both pressure and temp

Posted on April 03, 2018 at 00:53Hi guys,I have STEVAL-MKI183V1 connected to stm32l476rg NUCLEO. I have downloaded the C example code. Setup the SPI and the Interrupt pin using STM32CubeMX. With the help of some example code i hooked it all up. I ge...

0690X0000060AMaQAM.png 0690X0000060AJXQA2.png

Read\Write LIS2DH12 with I2C using DMA

Posted on November 17, 2017 at 15:13Hi, I am trying to read the LIS2DH12 using the I2C and DMA.I got everything configured via STM32CubeMx. When I want to read the LIS2DH12 (WHO_AM_I @0x0F) I call:HAL_I2C_Master_Receive_DMA(&hi2c1, (uint16_t)SLAVE_A...

dherbst by Associate
  • 1254 Views
  • 1 replies
  • 0 kudos

LIS2DH12 High Power consumption in normal power mode

Posted on April 18, 2018 at 15:42Hello,Currently,  am working with  lis2dh12 mem sensor for my ble application. I am using accelerometer to detect movement and then reading data from accelerometer using bypass mode. During no movement, the power con...

Unico: The adapter board has not been recognized.

Posted on April 19, 2018 at 02:10I am using a STEVAL-MKI109v2 with a STEVAL-MKI172v1 sensor board. When I run Unico 6.0.0.0 the MKI109v2 is not in the list of devices but the MKI172v1 is. When I select MKI172v1 and attempt to connect I get the follo...

spencer2 by Associate
  • 1483 Views
  • 1 replies
  • 0 kudos

Record microphone and motion sensors simultaneously

Posted on April 03, 2018 at 08:59I have a SensorTile Kit (STLKT01V1) running the http://www.st.com/content/st_com/en/products/embedded-software/mcus-embedded-software/stm32-embedded-software/stm32-ode-function-pack-sw/fp-sns-allmems1.htmlwhich I can...

LSM9DS1 Wake Up Interrupts

Posted on November 06, 2017 at 17:26The original post was too long to process during our migration. Please click on the attachment to read the original post.

Pastrana by Associate II
  • 2791 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.