2019-03-04 10:39 PM
Hi,
Based from the LSM303AGR CTRL_REG4 FS[1:0} Full Scale Selection are (00: ±2g; 01: ±4g; 10: ±8g; 11: ±16g).
I tried all settings and it is reversed. So, setting 00 is +-16g. So is this an error in the datasheet?
Regards,
Markel
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.