cancel
Showing results for 
Search instead for 
Did you mean: 

Current consumption enabling FSM on LSM6DSOX

f87
Associate II

Hi, how much is the additional current consumption enabling the FSM on LSM6DSOX? Regards

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Eleon BORLINI
ST Employee

Hi, it depends on the selected FSM ODR, number of FSM enabled, single FSM code.

Added power consumption is roughly estimated to be in the order of:

  • FSM ODR = 13 Hz --> (N + 1) * 1.5 uA
  • FSM ODR = 26 Hz --> (N + 1) * 2 uA
  • FSM ODR = 52 Hz --> (N + 1) * 3.5 uA
  • FSM ODR = 104 Hz --> (N + 1) * 6 uA

where N is the number of FSM enabled.

It is possible to measure the real current consumption only when a program is defined.

Regards

View solution in original post

2 REPLIES 2
Eleon BORLINI
ST Employee

Hi, it depends on the selected FSM ODR, number of FSM enabled, single FSM code.

Added power consumption is roughly estimated to be in the order of:

  • FSM ODR = 13 Hz --> (N + 1) * 1.5 uA
  • FSM ODR = 26 Hz --> (N + 1) * 2 uA
  • FSM ODR = 52 Hz --> (N + 1) * 3.5 uA
  • FSM ODR = 104 Hz --> (N + 1) * 6 uA

where N is the number of FSM enabled.

It is possible to measure the real current consumption only when a program is defined.

Regards

f87
Associate II

Thanks Eleon​

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.