MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM303C magnetometer automatic calibration not working in Android

I use a LSM303C magnetometer sensor on an Android platform.Sensor works fine, however automatic calibration (hard and soft iron) does not work. I checked it using an Android app displaying magnetic field vector in 2D, for both calibrated and uncali...

0690X000008BfSCQA0.png 0690X000008BfVaQAK.png
IGEHI by Associate
  • 3007 Views
  • 2 replies
  • 0 kudos

Help with programming the STM32 STEVAL-STLCS01V1 (with the STEVAL-STLKT01V1 Sensor development kit) using Arduino Uno sketch IDE.

I want to program the mcu STM32 STEVAL-STLCS01V1. I have the STEVAL-STLKT01V1 Sensor development kit and i've read that i can mount the STLCX01V1 on the Arduino Uno board, mount the STEVAL-STLCS01V1 on the STLCX01V1 board. and then use the Arduino sk...

RFink by Associate II
  • 1043 Views
  • 0 replies
  • 0 kudos

Need help getting initialized with MSP430F5529 to lsm303agr using STMems_Standard_C_Divers

 P4SEL |= 0x06;              // Assign I2C pins P4.1, P4.2 to USCI_B1 UCB1CTL1 |= UCSWRST;           // Enable SW reset UCB1CTL0 = UCMST + UCMODE_3 + UCSYNC;   // I2C Master, synchronous mode UCB1CTL1 = UCSSEL_2 + UCSWRST;      // Use SMCLK UCB1BR0 =...

JBonn by Associate III
  • 992 Views
  • 1 replies
  • 0 kudos

Is it possible to change the STEVAL-IDP005V1-GUI software files?

Hello everyone,I am conducting some tests with the STEVAL-BFA001V1B and STEVAL-IDP004V1 evaluation kit together with the STEVAL-IDP005V1 GUI software available on STSW-BFA001V1.But I need to make some changes in the STEVAL-IDP005V1-GUI software, the ...

Hertzing by Associate II
  • 1873 Views
  • 4 replies
  • 0 kudos

Resolved! STEVAL-MKI109V3 DfuSe update issue, no available DFU Device

Hello, I installed the latest driver version Unico 8.0.0. Now my board is shown in the decive manager.Ready to use.. Everything looks good.Now I am trying to update the FW in the STEVAL-MKI109V3 board. First I pressed the BT2 Button and pluged the US...

Chris0815 by Associate II
  • 1539 Views
  • 2 replies
  • 0 kudos

Generate Interrupt on horizontal rotation using LIS3DH

Hi,I have a jar lid which is equipped with LIS3DH accelerometer. The accelerometer is placed in the PCB such that the top layer of LIS3DH will face the sky in normal position. The jar has a groove for holding the lid and we need to put the lid in th...

IThom.5 by Associate II
  • 2672 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.