MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Sample product

Hello,i want to order a sample product iis2mdc because i don't find it available in any store.In my order it says "total price $0.00" and "subtotal: $0.00"but in the field "shipping cost: Estimate" in my country(Greece) has a shipping cost of $37.00....

0690X000008aGVxQAM.bmp 0690X000008aGY8QAM.bmp
ASIGA by Associate
  • 1129 Views
  • 2 replies
  • 0 kudos

LSM9DS1 - capacitors C1 and C5 allowed values

Hello.We are designing a HW with LSM9DS1 inertial chip. There are C1 capacitor recommended to be 100 nF and C5 to be 10 nF +- 10%, but we have not these values in our BOM so it would be an extra part type. Have these parts some allowed range of capac...

OHnil by Associate II
  • 2079 Views
  • 4 replies
  • 0 kudos

X-CUBE-MEMS1 Middleware initialization problem

Hi,I am using a Nucleo-F446RE board with an IFS01A2 to build an eCompass.I have built a project using CubeMX v5.2.1 and Atollic Truestudio v9.1.To start with I made sure that I was able to communicate with the different mems sensors and I am successf...

NHarb by Associate
  • 1666 Views
  • 2 replies
  • 0 kudos

VL53L1x motion feature enhancement

Hi. I want to use VL53L1x time-of-flight sensors in following scenarios:detect an empty hand and a hand with an item using gesture detection approach;detect the product movement up or down. Have done several tests to understand the dependence between...

KKoma by Associate
  • 863 Views
  • 0 replies
  • 0 kudos

LIS3DH read data not reasonable?

Hi I'm currently implementing a crash detector in our device. And it works quite fine, but I think the received values are not correct. The sensor is on a PCB which is already delivered and should be enabled as a new feature in the future. So they de...

capture by Associate
  • 2207 Views
  • 1 replies
  • 0 kudos

LIS2DH12TR accelerometer sensor

Hi ,I'm trying to read the accelerometer data from the LIS2DH12TR which is connected to CC1310 TI's Controller.In my design I'm using I2C hence i have connected the CS pin to Vdd(3.3V) and SA0 pin to VDD. As per the Data sheet with my case the addres...

LN by Associate II
  • 3044 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.