cancel
Showing results for 
Search instead for 
Did you mean: 

LSM9DS1 - capacitors C1 and C5 allowed values

OHnil
Associate II

Hello.

We are designing a HW with LSM9DS1 inertial chip. There are C1 capacitor recommended to be 100 nF and C5 to be 10 nF +- 10%, but we have not these values in our BOM so it would be an extra part type. Have these parts some allowed range of capacity to be selected from or these values are mandatory to proper function?

Thank you.

Ondrej

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Eleon BORLINI
ST Employee

​Hi Ondrej, aren't you able to find both of the capacitors C1 and C5 or only C5? While for the C1 a standard 0.22uF can be ok, the C5 is mandatory at 10nF. Which is the nearest to 10nF capacitance value available for you? Regards

OHnil
Associate II

Hi Elon.

Thank you for the fast answer. Now we have in our BOM:

100 uF, 18 pF, 4.7 uF, 470 nF.

So for C5 we place 10 nF, but for C1 is possible to place 470 nF / 0402?

Ondrej

Eleon BORLINI
ST Employee

​Hi Ondrej, ok for the 470nF value. Regards

OHnil
Associate II

Hi Eleon.

Thank you, perfect.

Ondrej

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.