cancel
Showing results for 
Search instead for 
Did you mean: 

what is the effect of mechanical shock and vibration on MotionFX sensor fusion library. What can go wrong if mems sensors placed on a cricket bat undergoing 30g force for few millis when ball hits the bat?

kasi viswanadh
Associate II

MotionFX,LSM6DSM,LSM303AGR,Sensor fusion,Mechanical Shock,Vibration

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Miroslav BATEK
ST Employee

Hi,

first of all what is your final applications?

I see several problems:

  • Most of the sensors has maximum range 16g so they want be able correctly measure 30g
  • I think the acceleration during the hit could be even higher than 30g, it will be very sharp high peak
  • If the sensor is not able to measure correctly the acceleration the sensor fusion won't be able to follow device position
  • The MotionFX is not designed for such a high acceleration so I think I will also filter high peaks
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.